The Unitary (UNT) Controller is an electronic device for digital control of packaged air handling units, unit ventilators, fan coils, heat pumps, and other terminal units serving a single zone or room. It can also be configured as a generic input/output device for basic point monitoring applications when used within a Metasys Network. You can easily configure point inputs and outputs and software features to control a wide variety of HVAC equipment applications. You may use the UNT as a standalone controller or connected to the Metasys Network through a Network Control Module (NCM) or Companion.
|